‎2025-06-04 12:53 AM - last edited on ‎2025-06-04 1:13 AM by Andrew Neil
Hello ST Team,
I am using STM32CubeIDE and working on STM32F072R8T6 MCU. I am not able to debug my code. Same code was working fine till few days. But now it give me follow error
Error: Data mismatch found at address 0x08001D99 (byte = 0x60 instead of 0x68)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
Please help me for the same. The error screen shot is as attached.
Best Regards,
Rakesh Gajjar
Solved! Go to Solution.
‎2025-06-04 3:37 AM
Hello Andrew
Tried the same code on another PC and it works fine. Now suggest me what should i do. Should i unistall the STM32CubeIDE and reinstall it again on problematic PC or any other suggestion ?
Best Regards,
Rakesh Gajjar
‎2025-06-04 1:19 AM
Welcome to the forum.
Please see How to write your question to maximize your chances to find a solution for best results; in particular, please give full details of your target hardware, what programmer you're using, etc.
@RakeshGajjar wrote:Error: Data mismatch found at address 0x08001D99 (byte = 0x60 instead of 0x68)
Error: Download verification failed
"Verification" is where the programmer reads-back the data from the MCU, and checks that it matches the file that was down loaded.
The message tells you that this check failed: it found the byte value 0x60 at address 0x08001D99, but that address should contain the value 0x68.
@RakeshGajjar wrote:Same code was working fine till few days.
Something must have changed ...
‎2025-06-04 1:26 AM
Thanks Andrew for prompt response.
I am using STM32F072R8T6 MCU with inhouse develop board for UPS Display application.
I am using SWD debugging Interface and ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32
The source code is same and no changes has been done.
It was working before and now i am not able to debug the same.
Please guide me.
Best Regards,
Rakesh Gajjar
‎2025-06-04 1:47 AM
@RakeshGajjar wrote:STM32F072R8T6 MCU with inhouse develop board
So you need to show the schematic; again, please see: How to write your question to maximize your chances to find a solution
@RakeshGajjar wrote:ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32
Can it still program other targets?
@RakeshGajjar wrote:UPS Display application.
possibilities for noise & damage?
‎2025-06-04 3:37 AM
Hello Andrew
Tried the same code on another PC and it works fine. Now suggest me what should i do. Should i unistall the STM32CubeIDE and reinstall it again on problematic PC or any other suggestion ?
Best Regards,
Rakesh Gajjar