cancel
Showing results for 
Search instead for 
Did you mean: 

Problems copying SWV log

tjcrone
Associate

I'm trying to copy data from the SWV Trace Log but when I try to copy over 1000 lines, Ctl-C brings up a "save as" dialog, and the data that are saved are corrupted with duplicated lines. It looks like there is a rounding error on the export so that lines are duplicated. Is there a CubeIDE setting that could fix this issue? Why does Ctl-C bring up "save as"? Any advice would help greatly. Thank you!

5 REPLIES 5
tjcrone
Associate

Copy and paste for SWV logs as well as the SWV Exception Timeline Graph seems to work fine in TrueStudio 9.3.0. I will be going back to TrueStudio until the numerous SWV bugs are worked out in CubeIDE. In the meantime, if anyone finds a solution to these issues please let us know. Cheers.

Cartu38 OpenDev
Lead II
Markus GIRDLAND
ST Employee

This should be fixed in the new release of CubeIDE which should be coming in the next few days, hopefully early next week. If it's still a problem after the release please let me know.

Good news! Thanks for update.​

Cartu38 OpenDev
Lead II

Works for me now based on fresh STM32CubeIDE 1.4.0 release.