cancel
Showing results for 
Search instead for 
Did you mean: 

Potential bug of STM32CubeIDE Version 1.9.0

PGius.1
Associate

Hi everyone, I don't know if this is the correct section, if not, I'm sorry, maybe you can move it to the correct section. I wanted to report a potential bug of STM32CubeIDE Version: 1.9.0, Build: 12015_20220302_0855 (UTC). The card I am using is the NUCLEO-L4R5ZI-P. I noticed that in this release going to configure an ADC and an SPI device, both with DMA, it is not possible to debug as every time I get the following annoying error: "Break at address" 0x1fff16e4 "with no debug information available, or outside of program code. ". I make this report as I solved it easily by going back to version 1.8.0 where this problem does not occur. I hope you can fix this soon so that I can install the new releases of the STM32CubeIDE. Thanks for the attention.

0 REPLIES 0