2024-04-02 2:34 PM
Hi,
I'm trying to set up the CDC with my H053RB board. and I found a guide on following link.
But I realized there was issue about HardFault_Handler. it happened all the time even though I commented out the ICACHE line as below.
MX_GPIO_Init(); //MX_ICACHE_Init(); MX_USART1_UART_Init(); MX_USART3_UART_Init(); MX_USB_PCD_Init(); /* USER CODE BEGIN 2 */ while(hUsbDeviceFS.pClassData == NULL); //HAL_Delay(8); // Minimum needed delay MX_ICACHE_Init(); /* USER CODE END 2 */
/* Infinite loop */ |
I'm wondering if there are any workaround for this issue.
Thanks,
Luke.
2024-04-02 3:13 PM
Hello @LukeJang522
I suggest you to take a look at this example. It should be helpful.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-02 5:17 PM - edited 2024-04-02 5:20 PM
STTwo-32,
Thank you for your reply.
I'm trying to generate the code that you sent the link, but there's errors.
1. there is no tx_api.h file.
app_threadx.h /* Includes ------------------------------------------------------------------*/ #include "tx_api.h" |
2. even I copy the file forcibly, there are another errors as below
In file included from ../Core/Src/app_threadx.c:22: ../Core/Inc/app_threadx.h:64:1: error: unknown type name 'UINT' 64 | UINT App_ThreadX_Init(VOID *memory_ptr); | ^~~~ ../Core/Inc/app_threadx.h:64:23: error: unknown type name 'VOID' 64 | UINT App_ThreadX_Init(VOID *memory_ptr); | ^~~~ ../Core/Src/app_threadx.c:59:1: error: unknown type name 'UINT' 59 | UINT App_ThreadX_Init(VOID *memory_ptr) | ^~~~ ../Core/Src/app_threadx.c:59:23: error: unknown type name 'VOID' 59 | UINT App_ThreadX_Init(VOID *memory_ptr) |
3. It seems like I can't just use the code, it might needs something else.
I wasn't also able to generate the code by UX_Device_CDC_ACM.ioc file.
I'm not sure there is another example or not. Could you please help me to fix it?
Thanks.
2024-04-04 3:16 PM
Hi @STTwo-32
I tried duplicating the code from the the link
Bt i seems that it never calls "entry function tx_application_define()". i've also chagne the "tx_initialize_low_level.S"
/* Set base of available memory to end of non-initialised RAM area. */ #ifdef USE_DYNAMIC_MEMORY_ALLOCATION LDR r0, =_tx_initialize_unused_memory // Build address of unused memory pointer //LDR r1, =Image$$RW_IRAM1$$ZI$$Limit // Build first free address LDR r1, =|Image$$RW_IRAM1$$ZI$$Limit| ADD r1, r1, #4 // STR r1, [r0] // Setup first unused memory pointer #endif |
Even I tried to connect USB to CN3.
Did I miss anything?
Thanks,