cancel
Showing results for 
Search instead for 
Did you mean: 

passing arguement 1 of 'HAL_RTC_GetTime' from incompatible pointer type

demir
Senior II

Hi,

I am getting the below warning when I compile my application. However, HAL_RTC_GetTime API expects the first argument of type pointer to a RTC_HandleTypeDef structure, thats what I provide, but I get this warning as highlighted below.

 

15:34:16 **** Incremental Build of configuration Debug for project RTC ****
make -j8 all 
arm-none-eabi-gcc "../Core/Src/main.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F407xx -c -I../Core/Inc -I../Drivers/STM32F4xx_HAL_Driver/Inc -I../Drivers/STM32F4xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"
../Core/Src/main.c: In function 'HAL_RTC_AlarmAEventCallback':
../Core/Src/main.c:337:49: warning: passing argument 1 of 'HAL_RTC_GetTime' from incompatible pointer type [-Wincompatible-pointer-types]
  337 |                                 HAL_RTC_GetTime(&hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);
      |                                                 ^~~~~
      |                                                 |
      |                                                 RTC_HandleTypeDef **
In file included from ../Core/Inc/stm32f4xx_hal_conf.h:391,
                 from ../Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal.h:29,
                 from ../Core/Inc/main.h:30,
                 from ../Core/Src/main.c:20:
../Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal_rtc.h:714:54: note: expected 'RTC_HandleTypeDef *' but argument is of type 'RTC_HandleTypeDef **'
  714 | HAL_StatusTypeDef HAL_RTC_GetTime(RTC_HandleTypeDef *hrtc, RTC_TimeTypeDef *sTime, uint32_t Format);
      |                                   ~~~~~~~~~~~~~~~~~~~^~~~
../Core/Src/main.c:338:49: warning: passing argument 1 of 'HAL_RTC_GetDate' from incompatible pointer type [-Wincompatible-pointer-types]
  338 |                                 HAL_RTC_GetDate(&hrtc, &RTC_DateRead,RTC_FORMAT_BIN);
      |                                                 ^~~~~
      |                                                 |
      |                                                 RTC_HandleTypeDef **
In file included from ../Core/Inc/stm32f4xx_hal_conf.h:391,
                 from ../Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal.h:29,
                 from ../Core/Inc/main.h:30,
                 from ../Core/Src/main.c:20:
../Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal_rtc.h:716:54: note: expected 'RTC_HandleTypeDef *' but argument is of type 'RTC_HandleTypeDef **'
  716 | HAL_StatusTypeDef HAL_RTC_GetDate(RTC_HandleTypeDef *hrtc, RTC_DateTypeDef *sDate, uint32_t Format);
      |                                   ~~~~~~~~~~~~~~~~~~~^~~~
arm-none-eabi-gcc -o "RTC.elf" @"objects.list"   -mcpu=cortex-m4 -T"C:\Users\bjvyhb\OneDrive - PHINIA\Desktop\MCU\Workspace\RTOS_Workspace\RTC\STM32F407VGTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="RTC.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
Finished building target: RTC.elf
 
arm-none-eabi-size  RTC.elf 
arm-none-eabi-objdump -h -S RTC.elf  > "RTC.list"
   text	   data	    bss	    dec	    hex	filename
  16684	    112	   2408	  19204	   4b04	RTC.elf
Finished building: default.size.stdout
 
Finished building: RTC.list
 

15:34:19 Build Finished. 0 errors, 2 warnings. (took 2s.589ms)

 

 

 

Could anyone please help me resolve ?

Thank you.

 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
RTC_HandleTypeDef hrtc;

UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */



/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_RTC_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)

char* getDayofWeek(uint8_t number);

char msg[200] ={0};
char msg2[200]={0};
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */



  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_RTC_Init();
  MX_USART2_UART_Init();
  /* USER CODE BEGIN 2 */


  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */


  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.LSIState = RCC_LSI_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 50;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
  RCC_OscInitStruct.PLL.PLLQ = 7;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief RTC Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_RTC_Init(void)
{

  /* USER CODE BEGIN RTC_Init 0 */

  /* USER CODE END RTC_Init 0 */

  RTC_TimeTypeDef sTime = {0};
  RTC_DateTypeDef sDate = {0};
  RTC_AlarmTypeDef sAlarm = {0};

  /* USER CODE BEGIN RTC_Init 1 */

  /* USER CODE END RTC_Init 1 */

  /** Initialize RTC Only
  */
  hrtc.Instance = RTC;
  hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
  hrtc.Init.AsynchPrediv = 127;
  hrtc.Init.SynchPrediv = 255;
  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
  if (HAL_RTC_Init(&hrtc) != HAL_OK)
  {
    Error_Handler();
  }

  /* USER CODE BEGIN Check_RTC_BKUP */

  /* USER CODE END Check_RTC_BKUP */

  /** Initialize RTC and set the Time and Date
  */
  sTime.Hours = 0x12;
  sTime.Minutes = 0x0;
  sTime.Seconds = 0x15;
  sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
  sTime.StoreOperation = RTC_STOREOPERATION_RESET;
  if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }
  sDate.WeekDay = RTC_WEEKDAY_FRIDAY;
  sDate.Month = RTC_MONTH_APRIL;
  sDate.Date = 0x12;
  sDate.Year = 0x24;

  if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }

  /** Enable the Alarm A
  */
  sAlarm.AlarmTime.Hours = 0x12;
  sAlarm.AlarmTime.Minutes = 0x0;
  sAlarm.AlarmTime.Seconds = 0x15;
  sAlarm.AlarmTime.SubSeconds = 0x0;
  sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
  sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
  sAlarm.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY;
  sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
  sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
  sAlarm.AlarmDateWeekDay = 0x31;
  sAlarm.Alarm = RTC_ALARM_A;
  if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN RTC_Init 2 */

  /* USER CODE END RTC_Init 2 */

}

/**
  * @brief USART2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{

  /* USER CODE BEGIN USART2_Init 0 */

  /* USER CODE END USART2_Init 0 */

  /* USER CODE BEGIN USART2_Init 1 */

  /* USER CODE END USART2_Init 1 */
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 115200;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART2_Init 2 */

  /* USER CODE END USART2_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);

  /*Configure GPIO pin : PA0 */
  GPIO_InitStruct.Pin = GPIO_PIN_0;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /*Configure GPIO pins : PD12 PD13 PD14 PD15 */
  GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

  /* EXTI interrupt init*/
  HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(EXTI0_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc)
{

	printf("Alarm is triggered\n\r");
	HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);

	RTC_TimeTypeDef RTC_TimeRead;
	RTC_DateTypeDef RTC_DateRead;


				HAL_RTC_GetTime(&hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);
				HAL_RTC_GetDate(&hrtc, &RTC_DateRead,RTC_FORMAT_BIN);

				if(RTC_TimeRead.TimeFormat == 0)
				{
					printf("current time is: %02d:%02d:%02d AM\r\n",RTC_TimeRead.Hours,RTC_TimeRead.Minutes,RTC_TimeRead.Seconds);
				}
				else
				{
					printf("current time is: %02d:%02d:%02d PM\r\n",RTC_TimeRead.Hours,RTC_TimeRead.Minutes,RTC_TimeRead.Seconds);
				}



			//	sprintf(msg,"current time is: %02d:%02d:%02d\r\n",RTC_TimeRead.Hours,RTC_TimeRead.Minutes,RTC_TimeRead.Seconds);


				HAL_UART_Transmit(&huart2, (uint8_t*)msg,1,1000);


				//sprintf(msg2,"current date is:%02d-%02d-%02d-%s\r\n",RTC_DateRead.Month,RTC_DateRead.Date, RTC_DateRead.Year,getDayofWeek(RTC_DateRead.WeekDay));
				printf("current date is: %02d-%02d-%02d-%s\r\n",RTC_DateRead.Month,RTC_DateRead.Date,RTC_DateRead.Year,getDayofWeek(RTC_DateRead.WeekDay));
				HAL_UART_Transmit(&huart2, (uint8_t*)msg2,20,1000);


	HAL_Delay(2000);
	HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);

}


char* getDayofWeek(uint8_t number)

{
	char* weekday[] = {"monday","tuesday","wednesday","thursday","friday","saturday","sunday"};

	return weekday[number-1];
}



PUTCHAR_PROTOTYPE
{
  /* Place your implementation of fputc here */
  /* e.g. write a character to the USART1 and Loop until the end of transmission */
  HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFFFF);

  return ch;
}


void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

{
	RTC_TimeTypeDef RTC_TimeRead;
	RTC_DateTypeDef RTC_DateRead;


			HAL_RTC_GetTime(&hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);
			HAL_RTC_GetDate(&hrtc, &RTC_DateRead,RTC_FORMAT_BIN);

			if(RTC_TimeRead.TimeFormat == 0)
			{
				printf("current time is: %02d:%02d:%02d AM\r\n",RTC_TimeRead.Hours,RTC_TimeRead.Minutes,RTC_TimeRead.Seconds);
			}
			else
			{
				printf("current time is: %02d:%02d:%02d PM\r\n",RTC_TimeRead.Hours,RTC_TimeRead.Minutes,RTC_TimeRead.Seconds);
			}



		//	sprintf(msg,"current time is: %02d:%02d:%02d\r\n",RTC_TimeRead.Hours,RTC_TimeRead.Minutes,RTC_TimeRead.Seconds);


			HAL_UART_Transmit(&huart2, (uint8_t*)msg,1,1000);


			//sprintf(msg2,"current date is:%02d-%02d-%02d-%s\r\n",RTC_DateRead.Month,RTC_DateRead.Date, RTC_DateRead.Year,getDayofWeek(RTC_DateRead.WeekDay));
			printf("current date is: %02d-%02d-%02d-%s\r\n",RTC_DateRead.Month,RTC_DateRead.Date,RTC_DateRead.Year,getDayofWeek(RTC_DateRead.WeekDay));
			HAL_UART_Transmit(&huart2, (uint8_t*)msg2,20,1000);


}

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

It seems a conflict between the first input argument of the callback and the definition of the global rtc handle declared in the top of your main.c:

/* Private variables ---------------------------------------------------------*/
RTC_HandleTypeDef hrtc;
void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc)
{

	printf("Alarm is triggered\n\r");
	HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);

	RTC_TimeTypeDef RTC_TimeRead;
	RTC_DateTypeDef RTC_DateRead;


				HAL_RTC_GetTime(&hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);
				HAL_RTC_GetDate(&hrtc, &RTC_DateRead,RTC_FORMAT_BIN);

So remove & before hrtc from here:

			HAL_RTC_GetTime(&hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);
			HAL_RTC_GetDate(&hrtc, &RTC_DateRead,RTC_FORMAT_BIN);

Does it resolve your issue?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

It seems a conflict between the first input argument of the callback and the definition of the global rtc handle declared in the top of your main.c:

/* Private variables ---------------------------------------------------------*/
RTC_HandleTypeDef hrtc;
void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc)
{

	printf("Alarm is triggered\n\r");
	HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);

	RTC_TimeTypeDef RTC_TimeRead;
	RTC_DateTypeDef RTC_DateRead;


				HAL_RTC_GetTime(&hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);
				HAL_RTC_GetDate(&hrtc, &RTC_DateRead,RTC_FORMAT_BIN);

So remove & before hrtc from here:

			HAL_RTC_GetTime(&hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);
			HAL_RTC_GetDate(&hrtc, &RTC_DateRead,RTC_FORMAT_BIN);

Does it resolve your issue?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
LCE
Principal

input handle hrtc is already a pointer, so only remove the "&" for hrtc.

HAL_RTC_GetTime(hrtc, &RTC_TimeRead, RTC_FORMAT_BIN);

That is why I don't like HAL, as hrtc might be a handle, or a pointer to a handle.
In my C sources, pointers always start with "p", like phRtc, or pu32Var. 
It really helps to avoid these problems.

Note that the compiler was telling you that you were providing a pointer-to-pointer (double indirection):

AndrewNeil_0-1712323448699.png

 


@LCE wrote:

That is why I don't like HAL, as hrtc might be a handle, or a pointer to a handle.
In my C sources, pointers always start with "p", like phRtc, or pu32Var. 


It's not really the fault of HAL here.

This is in user code - so the user could have (should have?) chosen to use such a naming convention; eg,

void HAL_RTC_AlarmAEventCallback( RTC_HandleTypeDef *pHrtc )
{
	printf( "Alarm is triggered\n\r" );
	HAL_GPIO_TogglePin( GPIOD, GPIO_PIN_14 );

	RTC_TimeTypeDef RTC_TimeRead;
	RTC_DateTypeDef RTC_DateRead;

	HAL_RTC_GetTime( pHrtc, &RTC_TimeRead, RTC_FORMAT_BIN );
	HAL_RTC_GetDate( pHrtc, &RTC_DateRead, RTC_FORMAT_BIN );

 

Using the same name for a handle and a pointer as a function call argument - I've seen that in many Cube / HAL sources.