cancel
Showing results for 
Search instead for 
Did you mean: 

Parse HEX File to HAL_FLASH_PROGRAM()

Martini
Associate II

Hello everyone, I want to make bootloader, everything is done, but not working. 

 

1. I create two apps in STM32CubeIDE:

BOOTLOADER: 0x08000000

APPLICATION: 0x08020000

I did simple program and I jump from app to boot, and from boot to app (It's works fine).

 

2. I send (In next step using GSM) my hex lines using UART, and I receive it correct.

3.I get address, type, checksum from every lines and I parse only data bytes (I see in debug its working good).

4. I clear memory, and try to flash program   and just not working. 

When I parse hex file I skip the first line and two the last line (do not contain data). In every line I skip ":10100000" (length, address, type)

I don't know if I do this correctly.

Someone maybe know why the penultimate line have type 05, data like: 08023C25

What should I do? 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

If "data" is a uint32_t, it should be reversed compared to what is shown in the hex file.

0x08020000, data: 0x20030000

...

Isn't this easily verified? Try one way, if it's reversed in memory, then reverse it before writing.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

7 REPLIES 7

The format isn't particularly complex and is well documented. Perhaps decode in C on a PC. Check conversation to BIN file.

Check binary with your STM32 side loader.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Guru

https://en.wikipedia.org/wiki/Intel_HEX

 

If you feel a post has answered your question, please click "Accept as Solution".
Martini
Associate II

I compare the .bin file and .hex, data is the same.

I debug my program i I correct write data to flash  (exmaple in screen). 

But its not working maybe I do something wrong. 

Maybe i should write data as little endian? â€ƒ

My first data line is:
:10 0000 00 00000320010902086D08020873080208 B5

Its ok when I write for example: (look screen of debug)

0x08020000: data: 0x00000320

0x08020004: data 0x01090208

etc.

 

example data debug.png

hex and bin compare.png

 

TDK
Guru

Data in memory needs to be in the same order as in the file. The system is little endian so data should appear reversed when interpreting it as a uint32_t.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for answer. You are best.

I want to understand correctly. 

If I have first line:

:10 0000 00 00000320010902086D08020873080208 B5

Data is: 00000320 01090208 6D080208 73080208

Should I write like this?

0x08020000, data: 0x00000320

0x08020004, data: 0x01090208

0x08020008, data: 0x6D080208

0x0802000C, data: 0x73080208

 

 

 

TDK
Guru

If "data" is a uint32_t, it should be reversed compared to what is shown in the hex file.

0x08020000, data: 0x20030000

...

Isn't this easily verified? Try one way, if it's reversed in memory, then reverse it before writing.

If you feel a post has answered your question, please click "Accept as Solution".

You are the best TDK :) 

I wasn't sure, I had more problems, but your answer helped me - you have right.

Data in .hex file is Big Endian, and we have to change it to Little Endian.