2020-02-25 12:47 PM - last edited on 2025-02-11 3:24 PM by Andrew Neil
Could not determine GDB version using command: /opt/st/stm32cubeide_1.2.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.0.0.201904181610/tools/bin/arm-none-eabi-gdb --version
/opt/st/stm32cubeide_1.2.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.0.0.201904181610/tools/bin/arm-none-eabi-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or directory
Solved! Go to Solution.
2024-05-04 11:51 AM
my Ubuntu Version is 24.04 LTS
and its not working
2024-05-07 2:24 AM
Thank you, still working on Ubuntu 24.04
2024-08-09 4:01 AM
Many thanks very usefull
2024-09-12 6:44 AM
Thanks! Adding the repository was the solution for me.
Hope ST fixes next versions in order to use libncurses6
2024-10-03 8:33 AM
I'm getting the same error but when I try the above command I get "unable to locate package libncurses5"????
2024-10-04 7:52 AM
ST has a real problem here as evidenced by the number of respondents. What needs to happen ASAP is a rebuild using libncurses.so.6. Looking across the net, it appears that 6 alleviates some long existing security issues. Version 5 is not even on option in my Mint/Ubuntu 22 Kernel 6.8 distribution. I finally resulted begrudgingly, to drop back to windows.
Good Luck All.
2024-10-04 7:54 AM
Object-Option not available in my distribution.
2025-01-14 9:53 AM
Your "ugly" workaround still much better than the ST "work" - still using the 12 year old libncurses5 .
(That can be installed no more ... apt get responds : : No installation candidate exists for package 'libncurses5'. )
So with gdb-multiarch IDE 1.17.0 has working debug again...great job !
2025-02-11 3:10 PM
Work for me: ubuntu 24.04 LTS:
- installed gdb-multiarch
- And as described :
sudo -i apt install gdb-multiarch # as mentioned before
cd /opt/st/stm32cubeide_1.15.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.linux64_1.0.100.202403111256/tools/bin # or wherever you installation is
mv arm-none-eabi-gdb arm-none-eabi-gdb.bak
ln -s /usr/bin/gdb arm-none-eabi-gdb
- Work for me in a VM.
- Thank you for the help
2025-02-22 11:58 PM
This solution doesn't seem to work for me. All MCUs enter reset loop when used with the gdb that comes with gdb-multiarch.