cancel
Showing results for 
Search instead for 
Did you mean: 

On ubuntu; debug says "Could not determine GDB version"

DQuir.1
Associate II

Could not determine GDB version using command: /opt/st/stm32cubeide_1.2.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.0.0.201904181610/tools/bin/arm-none-eabi-gdb --version

/opt/st/stm32cubeide_1.2.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.0.0.201904181610/tools/bin/arm-none-eabi-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or directory

 

44 REPLIES 44

my Ubuntu Version is 24.04 LTS 

and its not working 

 

Screenshot from 2024-05-04 21-48-10.png

 

Thank you, still working on Ubuntu 24.04

Many thanks very usefull

Thanks! Adding the repository was the solution for me.

Hope ST fixes next versions in order to use libncurses6

I'm getting the same error but when I try the above command I get "unable to locate package libncurses5"????

 

DAldr.1
Associate II

ST has a real problem here as evidenced by the number of respondents.  What needs to happen ASAP is a rebuild using libncurses.so.6.  Looking across the net, it appears that 6 alleviates some long existing security issues.  Version 5 is not even on option in my Mint/Ubuntu 22 Kernel 6.8 distribution.  I finally resulted begrudgingly, to drop back to windows.

 

Good Luck All.

Object-Option not available in my distribution.

Your "ugly"  workaround still much better than the ST "work" - still using the 12 year old libncurses5 .

(That can be installed no more ... apt get responds : : No installation candidate exists for package 'libncurses5'. )

So with gdb-multiarch IDE 1.17.0 has working debug again...great job !

If you feel a post has answered your question, please click "Accept as Solution".
vgoosse31
Associate

Work for me: ubuntu 24.04 LTS:

- installed gdb-multiarch

- And as described :

sudo -i apt install gdb-multiarch # as mentioned before

cd /opt/st/stm32cubeide_1.15.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.linux64_1.0.100.202403111256/tools/bin # or wherever you installation is

mv arm-none-eabi-gdb arm-none-eabi-gdb.bak

ln -s /usr/bin/gdb arm-none-eabi-gdb

 - Work for me in a VM.

- Thank you for the help

This solution doesn't seem to work for me.  All MCUs enter reset loop when used with the gdb that comes with gdb-multiarch. 

Screenshot From 2025-02-22 23-58-23.png