cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-H563 Getting Started Fails

chrisnielsen9
Associate III

Sorry for the newbie noise, but the website under Nucleo-H563ZI points me to a Getting Started document, UM1727, that is dated Jan 2016, and appears to no longer match current software tools.  Is there a replacement?

My initial goal is to simply rebuild the standard app shipped in the Nucleo, download it, and see the same LED blinking, then add from there.

Thank you, Chris

1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

>>no video (that I could find) exists on st.com for IDE basics

There are tons in fact! But I would highly suggest this one from MOOC (massive open online courses) STM32CubeIDE basics - STMicroelectronics 

>>Does a known to work rebuild project for Nucleo-H 563ZI exist? (to just "Hello World" == blink an LED, shipped app)

There are several projects on each peripheral (SPI, UART, DMA, TIM, FLASH,....) in the CubeFW that I've shared with you! 

For the patch, it should work either way, you can do it manually if that's what you're used to! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

12 REPLIES 12
Sarra.S
ST Employee

Hello Chris, welcome back!

That user manual (UM1727) is a generic guide for all Nucleo boards, what you're looking for instead is STM32H5 Nucleo-144 board (MB1404) user manual (UM3115)

Tip: you can always find the specific user manual of your board by searching the MB reference number printed on the Nucleo board, in this case it's MB1404. 

To get started with some projects, you can download the STM32H5 CubeFW package, where you can find some blinky project. 

Or start your application from configuring STM32cubeMX and then adding your code! check STM32StepByStep:Step2 Blink LED - stm32mcu

BR, 

Sarra.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you for the reply.  The Step2 link led me to Step1, which gives this install list:

  • STM32CubeMX, a tool to set and graphically program all STM32 boards and products
  • STM32CubeIDE, the free IDE to develop the STM32 software
  • STM32CubeProg, a tool to load/spy software in the STM32 memory
  • STM32CubeL4, an STM32L4 MCU software package with embedded examples

However, the IDE documentation now says that it incorporates some/all of the other tools.  I fear getting into install conflicts.  Is the above list still correct, or does installing the IDE give me all needed functionality?

Here are the links you need to install 

STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics (latest version is V6.13) 

STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics (latest version is 1.17) 

STM32CubeProg - STM32CubeProgrammer software for all STM32 - STMicroelectronics (you may not need this tool for now) 

STM32H5 MCU software package with embedded examples (since you have a Nucleo H5, the provided example is based on an L4 but can be tailored on a H5)  

There will not be any conflicts between software. The IDE has a CubeMX built-in version, but we mostly use CubeMX standalone. Either way, it will point to the same path, so there will not be an issue. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

All went well except for the software package.  There isn't an installer, just raw code, which I placed in a randomly named directory.  The link also shows Patch 1.1.1.  Do I manually need to drop the patch files on top of the other files, or is there some mechanism in the IDE where I tell it where I placed the code, then it checks for updates? (patches)

I might have found it.  Instead of using the 4th link in your reply for the H5 software, should I do this? :

- in the IDE, Help->Configuration Tool->Manage Embedded Software Packages

- select STM32H5, latest (1.4.0), then Install

Then I'm guessing the IDE can check for updates, and I can ignore the st.com Patch link?

The above seemed to go ok for the H5 software 1.4.0 install.  Questions:

1. Regarding Patch 1.1.1 install: I open IDE, then Help->STM32Cube updates->Check for Embedded Software Packages Updates, but it shows no updates available, and I know st.com has Patch 1.1.1 available.  How can I make the patch install, and how to check the installed version of the Software Packages after all installs/updates/patches complete?  This is important to ensure I have all the latest bug fixes.

2. I'd then like to browse the full software package for H5.  Can you share where it has been placed on my C: drive?  I've hunted all the ST directories and can't find it.

On #2, I found it: (would still like to know about #1)

C:\Users\CHNIELSE2001\STM32Cube\Repository\STM32Cube_FW_H5_V1.4.0\Projects\NUCLEO-H563ZI\Examples_LL\GPIO\GPIO_InfiniteLedToggling_Init\STM32CubeIDE\Application

The Wiki "StepByStep" still fails.  I press Run, and it fails for "No Configuration".  I'll go hunting for other tutorials and/or videos, but would be nice to hear your thoughts, as it is likely to be faster than my path.

Thank you

On Run/Debug Configuration, I watched all the Basics videos, no luck.  Strangely, no video (that I could find) exists on st.com for IDE basics, but I found one with an open web search on YouTube:

STM32CubeIDE - Launch configuration

This might also be needed/useful:

STM32CubeIDE - GDB server and probe configuration

I still haven't figured it out, but I think/hope I'm in the right area.  Help would still be appreciated.

Or, I suppose I could rephrase my ask without all of the above:

Does a known to work rebuild project for Nucleo-H563ZI exist? (to just "Hello World" == blink an LED, shipped app)