2025-02-07 3:39 AM - edited 2025-02-07 3:41 AM
Hello,
I can create a simple program in STM32CubeIDE V1.17.0 targeting the NUCLEO-G474RE board. I can build ok but am having problems with the GDB server starting.
JP5 is set to 5V_USB_STLK and JP (BOOT0) is off. I can do the ST-Link Upgrade without problem, so the USB cable and powering is ok.
I select Run>Run As>STM32 C/C++ Application and get the following.
STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
ST-LINK Failed to get target status
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
Solved! Go to Solution.
2025-02-07 6:07 PM
2025-02-07 11:14 AM - edited 2025-02-07 11:14 AM
Hello @alw ,
Have you tried the latest release of STM32CubeProgrammer?
Dd you change the default Option Bytes with Cubeprogrammer ?
Try connecting in "under reset" mode, then connect the debugger.
Check that the headers/jumpers on the Nucleo are fitted correctly.
Please follow the tips in this article : How to solve connection errors when connecting and... - STMicroelectronics Community
2025-02-07 6:07 PM
Hello,
Problem solved, it was just JP6 that was missing.