cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to run FreeRtos task with trustZone enabled

Kendall7
Associate II

Hi ,

I am trying to implement FreeRtos in my application with TrustZone enabled.

I want to blink LED1 in task1 and LED2 in task2.

Neither of the task are running.

When I did the debugging in function xTaskCreate it's going into Infinite loop.

My configuration:

FreeRtos-Nonsecure

Stack-128

Heap4

LED1-Nonsecure

LED2-NonSecure

I have attached my configuration and piece of code w.r.t task. 

I request anyone to help me resolve this issue .

 

void MX_FREERTOS_Init(void) {

/* USER CODE BEGIN Init */



/* USER CODE END Init */



/* USER CODE BEGIN RTOS_MUTEX */

/* add mutexes, ... */

/* USER CODE END RTOS_MUTEX */



/* USER CODE BEGIN RTOS_SEMAPHORES */

/* add semaphores, ... */

/* USER CODE END RTOS_SEMAPHORES */



/* USER CODE BEGIN RTOS_TIMERS */

/* start timers, add new ones, ... */

/* USER CODE END RTOS_TIMERS */



/* USER CODE BEGIN RTOS_QUEUES */

/* add queues, ... */

/* USER CODE END RTOS_QUEUES */

/* creation of Task1blink */

Task1blinkHandle = osThreadNew(LEDBlink1, NULL, &Task1blink_attributes);



/* creation of Task02 */

Task02Handle = osThreadNew(blinkled02, NULL, &Task02_attributes);



/* USER CODE BEGIN RTOS_THREADS */

/* add threads, ... */

/* USER CODE END RTOS_THREADS */



/* USER CODE BEGIN RTOS_EVENTS */

/* add events, ... */

/* USER CODE END RTOS_EVENTS */



}

/* USER CODE BEGIN Header_LEDBlink1 */

/**

* @brief Function implementing the Task1blink thread.

* @PAram argument: Not used

* @retval None

*/

/* USER CODE END Header_LEDBlink1 */

void LEDBlink1(void *argument)

{

/* USER CODE BEGIN Task1blink */

/* Infinite loop */

for(;;)

{

Toggle_Pin2();

osDelay(100);

}

/* USER CODE END Task1blink */

}

Kendall7_0-1711715069133.png

 

2 REPLIES 2
SofLit
ST Employee

Hello,


FreeRtos-Nonsecure

LED1-Nonsecure

LED2-NonSecure


I'm not Security feature expert by why you are enabling TrustZone while your application is non-secure?

And if you disable TrustZone are you facing the same issue?

PS: next time please use </> button to insert your code.

Thanks.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Kendall7
Associate II

Hi,

Thank you for replying to my post.

I am not facing this issue when trustZone is disabled.I am able to run FreeRtos without trustZone.

I am enabling TrustZone in non-secure because I want my product to be UL certified.I want two partition one for critical and non-critical ,Since trustzone enabling gives me two Independent hex files I am trying to run freeRtos in Non-secure region.