cancel
Showing results for 
Search instead for 
Did you mean: 

No such file or directory ?

bnymntrz
Associate III

Hi guys! I have a trouble about STMCubeIDE, I installed and created a project, Later, I received this two error ;

c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: cannot open linker script file C:\Users\B??nyamin Terzi\stm\mcu\001MCU\STM32F407VGTX_FLASH.ld: No such file or directory

make: *** [makefile:63: 001MCU.elf] Error 1

If you can help me, I will be pleased.

1 ACCEPTED SOLUTION

Accepted Solutions

I solved the problem, The program wasn't finding the way, The problem has been solved after I created the file of project in C disk. thank you!

View solution in original post

3 REPLIES 3

Does the file ACTUALLY exist on the path/name listed?

T​ry using path names without non-ASCII characters.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Do you mean the character of file name ?

I solved the problem, The program wasn't finding the way, The problem has been solved after I created the file of project in C disk. thank you!