2024-01-10 02:34 AM - last edited on 2024-01-10 02:43 AM by Mike_ST
To whom it may concern,
I have seen comments of similar regard with this issue, however I have not seen a way to solve the problem. When I try to debug my code and transmit it to my STM32F407G-DISC1 board it comes up with this "No ST-Link detected issue". I have attached photos, any help would be greatly appreciated.
2024-01-10 02:38 AM
What is the silver box at the bottom? Only a part of your setup is visible, so maybe there is still some error in your setup. Did youtry to connect the board direct to the PC?
2024-01-10 02:44 AM - edited 2024-01-10 03:06 AM
Hello @JHunt12 and welcome to the ST Community 😊.
I suggest you to:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-10 02:56 AM
Don't use Hubs or Docking Stations.
Make sure to use a Data Cable not a Charging Cable