No ST-Link detected - Only in CubeIDE 1.13.2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-18 9:06 AM
Hi,
I'm getting an error "No ST-Link detected" with the CubeIDE 1.13.2.
I can detect the programmer in the device manager:
And I can connect and program the board (Nucleo L452RE-P) using the STM32CubeProgrammer.
I have recently updated from CubeIDE v1.7 to 1.13.2, I think this was the first time I fully restarted the laptop and it can't program the board after that.
Is this a known issue in this version of CubeIDE?
Is there any recommended work around?
Regards,
Joao
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-19 8:32 AM
Somehow I managed to get it back working (for now at least).
I noticed that the STLink Server installed was version 2.1.1, while on ST website, the latest version is 2.1.0. This 2.1.1 version should have been installed with the new IDE version but it's weird that not even ST lists it.
So, I uninstalled version 2.1.1 (via windows Add or Remove programs, but made a backup first) and installed the known 2.1.0 version. After a couple of reboots, seems to be working and I can now see the stlinkserver.exe in the task manager. If anything, it only seems a bit slower (but better than not working :) ).
Hopefully this is investigated and addressed with a new update to the IDE.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-19 1:14 AM - edited ‎2023-10-19 1:37 AM
It's a bit weird that the GDB Server in use seems to be from the previous installation, at least looking at the path used in the Debug configuration.
Looking at the Installation details, it seems like there's a mix between the new and the old installation.
Regards,
Joao
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-19 2:05 AM
Hello @jvieira88
And welcome to the Community!
For the installations details, it show the path of the installation that has not been changed
since you updated from CubeIDE v1.7 to 1.13.2,
for the STLink can you try to upgrade the STlink from Help>ST-Link Upgrade or verify your cable.
Thank you!
Souhaib
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-19 2:52 AM
Hi Souhaib,
The STLink upgrade works, it detects the St-link which is already at the latest version.
Regarding the mismatch in installation details from my previous reply, that was because I was running the 1.7 IDE (which shows version 1.13.2 and points at all the 1.7 version plugins). Opening version 1.13.2 IDE seems to show the version/paths that I was expecting.
It's weird that with the upgrade both versions coexist at the same time. The problem is still not fixed and I can't program the Nucleo board using the IDE. I've noticed in other posts people referring to the stlinkserver.exe process in the task manager, I cannot see this process here. I wonder if there is some conflict after the upgrade.
As mentioned before, this is not a cable issue. I can program the board just fine with the CubeProgrammer, this issue seems to be relate to the CubeIDE / stlink-server.
Regards,
Joao
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-19 8:32 AM
Somehow I managed to get it back working (for now at least).
I noticed that the STLink Server installed was version 2.1.1, while on ST website, the latest version is 2.1.0. This 2.1.1 version should have been installed with the new IDE version but it's weird that not even ST lists it.
So, I uninstalled version 2.1.1 (via windows Add or Remove programs, but made a backup first) and installed the known 2.1.0 version. After a couple of reboots, seems to be working and I can now see the stlinkserver.exe in the task manager. If anything, it only seems a bit slower (but better than not working :) ).
Hopefully this is investigated and addressed with a new update to the IDE.