cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE crashing on startup Ubuntu

Dabbo
Associate III

After having a problem with the generic Linux installation I uninstalled STM32CubeIDE and instead installed the Debian version. It loads up but when I click on File>New STM32 Project it says STM32 target or STM32CubeIDE example selection is required. Can't progress past that point. Log file attached

 

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Mahmoud Ben Romdhane
ST Employee

Hello @Dabbo,

Thank you for posting.

Can you share the .log file and provide a screenshot of the STM32CubeIDE issue.

Thanks.

Mahmoud.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.