cancel
Showing results for 
Search instead for 
Did you mean: 

No binary or hex file output

RAltm
Senior

Hello,

I've a strange problem with CubeIDE 1.6.0, there's no binary or hex file output even if the corresponding outputs are activated under MCU post build outputs. Any ideas what might be the issue there?

Regards

20 REPLIES 20

Hmm... that's the reason why I don't like Eclipse. Most IDEs are made of it, most functions of it are not used or unusable in the context for a given platform, it wastes space if you've several installations of different vendors, what works on one installation doesn't work on another... and it must be horrible for a vendor to customize it, I assume.

But, I think the question is answered and the problem solved - use external builder.

Thank you all.

Regards