cancel
Showing results for 
Search instead for 
Did you mean: 

Newbie here. I would like to use STM32CubeIDE to debug the Marlin 3D printer software running on a STM32F429 via an ST-Link. I don't want to compile. Pointers to the right docs to read, what project type to use, debug setup would be appreciated.

BKuhn
Associate III
 
11 REPLIES 11
BKuhn
Associate III

It took a bit but eventually I captured a brief popup saying "Progress information", "Preparing launch delegate." and "Performing final launch validation ..."

Nothing in the problems window or the build console.

I did find a checkbox that says "Log to file" but nothing gets written to the TXT file I pointed it at.

BKuhn
Associate III

All is well.

I uninstalled and re-installed STM32CubeIDE and now I can single step my program!

Many Thanks!

Bob