cancel
Showing results for 
Search instead for 
Did you mean: 

New and clean CubeIDE/MX project does not compile

HMüll.4
Senior

Hi,

I have just set up a fresh and clean STM32F466 project in CubeMX which makes use of a UART and a bunch of GPIOs. right after generating the code (and prior to changing ANYTHING at the generated code!), I get the following compile error in CubeIDE:

c:\st\stm32cubeide_1.11.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe:C:\F\motion\STM32F446RETX_FLASH.ld:88: non constant or forward reference address expression for section .ARM.extab

Any idea how to fix that?

Thanks!

 

1 ACCEPTED SOLUTION

Accepted Solutions
HMüll.4
Senior

OK, finally I found it: at this position there was a statement

(READONLY)

which does not seem to be supported by the GCC-version that comes with CubeIDE.

 

View solution in original post

4 REPLIES 4
TDK
Super User

Include the IOC file you are having issues with.

Ensure you're on the latest CubeMX version.

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Super User

What is in C:\F\motion\STM32F446RETX_FLASH.ld line 88 ?

 

HMüll.4
Senior

OK, finally I found it: at this position there was a statement

(READONLY)

which does not seem to be supported by the GCC-version that comes with CubeIDE.

 

It is supported in more recent toolchains for CubeIDE.