2024-06-11 04:34 AM
Hello,
After installing version 1.15.1 of CubeIDE, the labels in the column headers 'System Core/NVIC/Code generation' disappeared. It's not a big issue, but it's a bit annoying.
Look at the below image.
Solved! Go to Solution.
2024-06-11 04:51 AM
Hello @Xanadu
Try to uninstall then reinstall the STM32CubeIDE v 1.15.1 from the official ST site instead of using the option update.
I will be waiting for your feedback.
THX
Ghofrane
2024-06-11 04:41 AM
Hello @Xanadu
First let me thank you for posting.
I would appreciate it if you could tell me the operating system you are using.
THX
Ghofrane
2024-06-11 04:46 AM
Hello,
I'm using Windows 10 and Windows 11. The issue occurs on both.
2024-06-11 04:51 AM
Hello @Xanadu
Try to uninstall then reinstall the STM32CubeIDE v 1.15.1 from the official ST site instead of using the option update.
I will be waiting for your feedback.
THX
Ghofrane
2024-06-11 05:43 AM
OK! This is the solution.
I was wrong 'cos I thought the days were gone when all I had to do was uninstall and reinstall...
Thanks!