cancel
Showing results for 
Search instead for 
Did you mean: 

LPTIM does not count pulses from the COMP output

Valen_id
Associate II

I want to count the pulses coming from COMP2's output using LPTIM1. However, when I send it to Tera Term, the displayed LPTIM value is consistently 1, and it doesn't match the COMP2 output.

Has anyone had this problem? How did you resolve it?

I would greatly appreciate it if there is an expert who can assist in fixing this issue.

I am using STM32Cube IDE Version: 1.10.1.

My MCU is STM32L051C8T, on a custom board

This is my clock

Valen_id_0-1691160876385.png

This my LPTIM configuration

Valen_id_1-1691160953620.png

this COMP configuration

Valen_id_2-1691160988272.png

this my code

#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "lc_sensor_metering.c"
#include "stdio.h"
#include "stdint.h"
#include "string.h"
#include "stm32l0xx_hal.h"
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
LcSensor_Sensor_f LcSensor1;
LcSensor_LcStatus_f LcStatus;
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
uint8_t aMsgBuffer[50];
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
COMP_HandleTypeDef hcomp2;
 
LPTIM_HandleTypeDef hlptim1;
 
UART_HandleTypeDef hlpuart1;
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_COMP2_Init(void);
static void MX_LPTIM1_Init(void);
static void MX_LPUART1_UART_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
LcSensor1.CountDetect = 2;
  /* USER CODE END 1 */
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_COMP2_Init();
  MX_LPTIM1_Init();
  MX_LPUART1_UART_Init();
  /* USER CODE BEGIN 2 */
 
  HAL_COMP_Start(&hcomp2);
  uint32_t counterValue = HAL_LPTIM_ReadCounter(&hlptim1);
  //sprintf((char*) aMsgBuffer, "Batas deteksi:%d\r\n",counterValue);
  //HAL_UART_Transmit(&hlpuart1, aMsgBuffer, TXBUFFERSIZE(aMsgBuffer),0xFFFF);
  //HAL_UART_Transmit(&hlpuart1, "dua", 10, 1000);
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
HAL_LPTIM_ReadCounter(&hlptim1);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_3, SET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, SET);
LC_Init_GPIO();
// sprintf((char*) aMsgBuffer, "Batas deteksi:%d\r\n",LcSensor1.CountDetect);
// HAL_UART_Transmit(&hlpuart1, aMsgBuffer, TXBUFFERSIZE(aMsgBuffer),0xFFFF);
char buffer[50]; // Adjust the buffer size based on your needs
sprintf(buffer, "counter value: %3lu\r\n", counterValue);
HAL_UART_Transmit(&hlpuart1, (uint8_t*) buffer, strlen(buffer), HAL_MAX_DELAY);
  HAL_Delay(1000);
//sprintf(buffer, "counter value: %lu\r\n", counterValue);
//HAL_UART_Transmit(&hlpuart1, (uint8_t*) buffer, strlen(buffer), HAL_MAX_DELAY);
 
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}
 
/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 
  /** Configure the main internal regulator output voltage
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
 
  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV16;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
  {
    Error_Handler();
  }
  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_LPUART1|RCC_PERIPHCLK_LPTIM1;
  PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1;
  PeriphClkInit.LptimClockSelection = RCC_LPTIM1CLKSOURCE_PCLK;
 
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
  {
    Error_Handler();
  }
}
 
/**
  * @brief COMP2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_COMP2_Init(void)
{
 
  /* USER CODE BEGIN COMP2_Init 0 */
 
  /* USER CODE END COMP2_Init 0 */
 
  /* USER CODE BEGIN COMP2_Init 1 */
 
  /* USER CODE END COMP2_Init 1 */
  hcomp2.Instance = COMP2;
  hcomp2.Init.InvertingInput = COMP_INPUT_MINUS_IO1;
  hcomp2.Init.NonInvertingInput = COMP_INPUT_PLUS_IO3;
  hcomp2.Init.LPTIMConnection = COMP_LPTIMCONNECTION_IN1_ENABLED;
  hcomp2.Init.OutputPol = COMP_OUTPUTPOL_NONINVERTED;
  hcomp2.Init.Mode = COMP_POWERMODE_MEDIUMSPEED;
  hcomp2.Init.WindowMode = COMP_WINDOWMODE_DISABLE;
  hcomp2.Init.TriggerMode = COMP_TRIGGERMODE_NONE;
  if (HAL_COMP_Init(&hcomp2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN COMP2_Init 2 */
 
  /* USER CODE END COMP2_Init 2 */
 
}
 
/**
  * @brief LPTIM1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_LPTIM1_Init(void)
{
 
  /* USER CODE BEGIN LPTIM1_Init 0 */
 
  /* USER CODE END LPTIM1_Init 0 */
 
  /* USER CODE BEGIN LPTIM1_Init 1 */
 
  /* USER CODE END LPTIM1_Init 1 */
  hlptim1.Instance = LPTIM1;
  hlptim1.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
  hlptim1.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV1;
  hlptim1.Init.UltraLowPowerClock.Polarity = LPTIM_CLOCKPOLARITY_RISING;
  hlptim1.Init.UltraLowPowerClock.SampleTime = LPTIM_CLOCKSAMPLETIME_DIRECTTRANSITION;
  hlptim1.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE;
  hlptim1.Init.OutputPolarity = LPTIM_OUTPUTPOLARITY_HIGH;
  hlptim1.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE;
  hlptim1.Init.CounterSource = LPTIM_COUNTERSOURCE_EXTERNAL;
  if (HAL_LPTIM_Init(&hlptim1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN LPTIM1_Init 2 */
  if (HAL_LPTIM_Counter_Start(&hlptim1, 0xFFFF) != HAL_OK)
    {
      Error_Handler();
    }
  /* USER CODE END LPTIM1_Init 2 */
 
}
 
/**
  * @brief LPUART1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_LPUART1_UART_Init(void)
{
 
  /* USER CODE BEGIN LPUART1_Init 0 */
 
  /* USER CODE END LPUART1_Init 0 */
 
  /* USER CODE BEGIN LPUART1_Init 1 */
 
  /* USER CODE END LPUART1_Init 1 */
  hlpuart1.Instance = LPUART1;
  hlpuart1.Init.BaudRate = 9600;
  hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
  hlpuart1.Init.StopBits = UART_STOPBITS_1;
  hlpuart1.Init.Parity = UART_PARITY_NONE;
  hlpuart1.Init.Mode = UART_MODE_TX_RX;
  hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&hlpuart1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN LPUART1_Init 2 */
 
  /* USER CODE END LPUART1_Init 2 */
 
}
 
/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
 
  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1|GPIO_PIN_3, GPIO_PIN_RESET);
 
  /*Configure GPIO pins : PA1 PA3 */
  GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_3;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

 

13 REPLIES 13

But why my counter value displayed in the serial terminal remains 1, do you know it

Valen_id_0-1691368297323.png

This is my code 

Valen_id_1-1691368364054.png

 

Where do you change the counterValue variable?

JW

Do you mean my variable is on line 107

Yes. You don't change it in the while() loop.

JW