2022-01-12 5:48 AM
Hi Guys,
I'm writting a bootlader/application for STM32L4 in STM32CubeIDE i I want my app to run even if there is no bootloader in memory.
This is my *.ld file:
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 96K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x8001000, LENGTH = 1024K-0x1000
BOOT (rx) : ORIGIN = 0x8000000, LENGTH = 131K
}I my app source I have the below function (which is properly placed at 0x8000000 in flash) :
#define MY_BL_FUNCTIONS __attribute__((section(".bootsection")))
void __attribute__((optimize("O0"))) Bootloader_JumpToApplication(void); MY_BL_FUNCTIONS
void __attribute__((optimize("O0"))) Bootloader_JumpToApplication(void)
{
asm("ldr R0,=0x8001004"); //my app start address
asm("BX R0"); //jump to app
}Unfortunately asm("BX R0") makes a sudden jump to my HardFault_Handler. instead of 0x8001004.
What do I do wrong?
Thanks in advance
Tom
2024-06-19 12:34 PM
>>Any solution?
Yeah, code like you're running on a Cortex-M4F.. rather than FAFO