cancel
Showing results for 
Search instead for 
Did you mean: 

ioc configuration-->system core--> NVIC--> CODE generation is empty???

JSING.1
Associate

i am using STM32F407G on STM32CUBEIDE.Untill yesterday my IDE was working properly but yesterday evening i came across a very strange error. i dont know whether i should call it error or not bcz its not actually not an error.

when i created a new project and went for ioc configuration,in the NVIC section the code generation(which is usually filled up with 7-8 entries) is completely empty. i checked all my projects on the IDE...in each IOC, Code generation part of NVIC is completely empty. i have also shared a screenshot. can someone help me??

0693W00000SwBWuQAN.png

2 REPLIES 2
Semer CHERNI
ST Employee

Hello @JSING.1​ 

First let me thank you for posting.

Could you provide me with the version of the tools you are using : The CubeIDE and CubeMx.

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

lonejack
Associate III

I've the same problem. Project built (ex-novo) for NUCLEO H755ZI. On NVIC1/2 -> code generation -> screen empty, no options

My mistake. I see the generation tab. Necessary to enlarge the view area.