2023-07-12 12:12 AM
Hi,
i want to clone my project. I did the following steps:
1) Edit > Copy.
2) Edit > Paste.
3) Rename the ioc files.
4) Delete the Debug.launch file.
5) Project > Clean.
the next step is to generate the CubeMX. But when I try to open the .ioc file this error message occurs:
Invalid Input: Must be project's active .ioc file.
can anybody help me please?
2023-07-13 11:49 PM
Hi Peter,
I opened the project with the newest STM32CubeIDE and migrated it to the newest firmware.
It works and I can open the .IOC file now after copy and paste the project.
Thanks for your help Peter!
2023-07-14 03:14 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Regards
/Peter