I2C communication issue when called from UART Command line
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-03 4:27 AM - edited ‎2024-06-03 5:57 AM
Hi There,
we have an IO Expender connected to I2C2, We read the GPIO using function "Read_IOExpendr2_Status();"
also, we have a UART connection for CLI
the function "Read_IOExpendr2_Status();" is at "Application.c" file
the CLI is at "COM_PORT.c" File
when the costumer send any UART message, a function is activated "void executeSerialCommand1(char *uart1RxBuf)"
inside that function there is a call for Read_IOExpendr2_Status();
CODE: (COM_PORT)
void executeSerialCommand1(char *uart1RxBuf)
{
Read_IOExpendr2_Status();
}
CODE: (MAIN)
void Read_IOExpendr2_Status(void)
{
uint8_t pRegAddress[2] = {INPUT_PORT0,INPUT_PORT1};
pcal9555_readRegister(&hi2c2, (uint16_t)PCAL9555_I2C_ADD_2, pRegAddress,USB_Link_Status );
}
Declaration of: pcal9555_readRegister
HAL_StatusTypeDef pcal9555_readRegister(I2C_HandleTypeDef *hi2c, uint16_t address, uint8_t *pRegAddress, uint8_t *pData);
Definition of: pcal9555_readRegister
HAL_StatusTypeDef pcal9555_readRegister(I2C_HandleTypeDef *hi2c, uint16_t address, uint8_t *pRegAddress, uint8_t *pData){
//Set the register address in the pointer register
HAL_Status = pcal9555_writeRegister(hi2c, address, pRegAddress, 1);
HAL_Status= HAL_I2C_Master_Receive_IT(hi2c, address, pData, 1);
while (HAL_I2C_GetState(hi2c) != HAL_I2C_STATE_READY){
/* Error_Handler() function is called when Timeout error occurs.
When Acknowledge failure occurs (Slave don't acknowledge its address)
Master restarts communication */
if ((HAL_I2C_GetError(hi2c) != HAL_I2C_ERROR_AF)&&(HAL_I2C_GetError(hi2c) != HAL_I2C_ERROR_NONE))
{
Error_Handler();
}
}
return HAL_Status;
}
the result is that the MCU send the IO Expender's address and then SDA and SCL lines set to '1' constant
from debugging, i can see that there is an issue with "pData"
HAL_Status = HAL_I2C_Master_Transmit_IT(hi2c,address, pData, Size);
when the function "Read_IOExpendr2_Status();" is called Outside of "void executeSerialCommand1(char *uart1RxBuf)" the value of pData is 0x200008F8
when the function "Read_IOExpendr2_Status();" is called Inside of "void executeSerialCommand1(char *uart1RxBuf)" the value of pData is 0x20000668
the Program enters a loop
while (HAL_I2C_GetState(hi2c) != HAL_I2C_STATE_READY)
MCU: STM32F072CBU6
any suggestions?
thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-03 4:38 AM
The two functions have different static buffers.
Not sure this can be solved via the description, attach more salient portions of the source.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-03 5:39 AM
thank you, i have updated the post with relative code
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-03 5:47 AM - edited ‎2024-06-03 5:47 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-03 5:56 AM
thank you, i didn't find it at first
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-03 6:06 AM - edited ‎2024-06-03 6:28 AM
You need to re-do the indentation!
void Read_IOExpendr2_Status(void) //USB/ETH LINK[1-5] on IOE IOs P.0[0-4]
{
uint8_t pRegAddress[2] = {INPUT_PORT0,INPUT_PORT1};
pcal9555_readRegister( &hi2c2, (uint16_t)PCAL9555_I2C_ADD_2, pRegAddress,USB_Link_Status );
}
So pRegAddress is a local, automatic (or "auto") variable.
This means that a new instance of that variable is created on the stack each time the function is called.
Therefore the address would be expected to change.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-26 6:24 AM
hi there,
i have replaced the pRegAddress to global variable
same results
i have uploaded a more detailed topic with more code and more tests at this link:
https://community.st.com/t5/stm32-mcus-products/i2c-issue-when-called-from-external-file/td-p/689715