cancel
Showing results for 
Search instead for 
Did you mean: 

I got an error in my drivers(src) part. it is visible in the picture which I attached

MFara.4
Associate III

I just started CubeIDE and I use macOS. I think there is a missing in installation as error is in driver part (Src)

4 REPLIES 4
ABIZO.1
Associate II

Which type is this error ? Can you show the complete error ?

MFara.4
Associate III

I ran the code in the windows it works properly but on my macOS system there is a red error on Drivers part. Please find the picture of that part in attachment.

ABIZO.1
Associate II

All the files in red are a double. You can see "stm32g0xx_hal_cortex.c" and "stm32g0xx_hal_cortex 2.c". I think you can remove all files number 2.

yes it is working now. thank you :folded_hands: