2022-12-02 12:09 AM
I just started CubeIDE and I use macOS. I think there is a missing in installation as error is in driver part (Src)
2022-12-02 12:16 AM
Which type is this error ? Can you show the complete error ?
2022-12-02 12:28 AM
2022-12-02 12:49 AM
All the files in red are a double. You can see "stm32g0xx_hal_cortex.c" and "stm32g0xx_hal_cortex 2.c". I think you can remove all files number 2.
2022-12-02 01:21 AM
yes it is working now. thank you