cancel
Showing results for 
Search instead for 
Did you mean: 

how to use UART2 independently - isolated from ST link. STM32103RB

Dadhichee_19
Associate II

i have STM32103RBT6, i want to use all three UARTs for a project. i want to use UART2 thorugh PA2 and PA3. 

The connection are : SB61, SB62 and SB63 are open. SB13 & SB14 are open as well. Continuity is there between SB62 & SB62 to TX on ST link (from track side) & between SB63 to RX on ST link (from track side). No continuity between  PA2 and PA3 with SB13 & SB14. can anyone tell me how to use UART2 from the PA2 and PA3? i want to use it for modbus but the transmission is failing. 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

It seems you are using NUCLEO-F103RB.

And this is what is said in the user manual UM1724:

mALLEm_0-1741160580877.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

You didn't mention which board you are using!

And this is not related to CubeIDE. The post need to be moved to hardware boards forum board.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

It seems you are using NUCLEO-F103RB.

And this is what is said in the user manual UM1724:

mALLEm_0-1741160580877.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you so much my friend. Big help here. sometimes we overlook highlighted details. Thanks