cancel
Showing results for 
Search instead for 
Did you mean: 

How to set Rank of A/D inputs for a L031 chip using the STM32CubeIDE?

RCooke88
Senior

Hi Folks,

All of the examples I see online show that in the CubeIDE there is a selection to enter the rank of the A/D inputs. I can't find that in my version which I believe is the latest version. Can someone point me to how I should accomplish this?

I'm using IN5, IN6, IN8 and IN9. I want to use DMA and read the values once per call to a function.

Thanks,

Richard

 

1 REPLY 1
MM..1
Chief III

Some ADC order ranks by channel order, cant change.