2019-04-30 4:52 AM
Trying out the new STM32CubeIDE. Mostly, I like it. There are some rough edges and dialogues that do not behave properly (at least on the Mac) but the thing I cannot make work is to add a 'Run' configuration to the toolbar.
I want to just build the code and flash it without having to open the Debug Perspective.
The preferences indicate that he options should be there but hey do not show in the toolbar.
Any ideas?
Solved! Go to Solution.
2020-07-29 9:23 AM
Only the OP can tag a topic/thread answered.
2020-07-29 11:09 AM
Well maybe you can try the mbed way: STLink behave as USB memory stick, so if you can generate the BIN file, you might be able to simply drag and flash using any file explorer... until the CubeIDE has one click provision to do so.
2020-07-29 2:32 PM
Can't for the life of me see how to do that. Sorry.