2019-04-30 4:52 AM
Trying out the new STM32CubeIDE. Mostly, I like it. There are some rough edges and dialogues that do not behave properly (at least on the Mac) but the thing I cannot make work is to add a 'Run' configuration to the toolbar.
I want to just build the code and flash it without having to open the Debug Perspective.
The preferences indicate that he options should be there but hey do not show in the toolbar.
Any ideas?
Solved! Go to Solution.
2020-07-29 6:40 AM
Since 1.3.0 run mode is supported. Just select your project within project explorer then:
2019-04-30 8:29 AM
This wasn't implemented in 1.0 as we didn't have time, but it's planned to get implemented at a later point.
For now you can go to the debug configuration to the "Startup" tab and put "quit" in the Run Commands box.
It's the closest thing to a workaround for now.
2019-04-30 1:54 PM
Ah - OK. Thanks for getting back with that.
At the risk of pushing my luck, what does your release schedule look like?
2019-05-06 1:48 AM
I can't share that, I'm afraid. The schedule also changes quite frequently depending on new demands/requests and I don't want to disappoint people by saying a date which we then don't release at.
2019-05-08 6:43 AM
for me, only adding "quit" did not work out with Segger GDB tool. here is what I needed to add:
2020-07-29 6:10 AM
I am on v1.4, is there any update on whether this feature has been added yet?
2020-07-29 6:40 AM
Since 1.3.0 run mode is supported. Just select your project within project explorer then:
2020-07-29 9:10 AM
Ah I see, thanks. That wasn't very clear to me as usually it is called "flash" or "download" but I guess eclipse is designed more for C++ PC applications rather than a dedicated embedded IDE.
2020-07-29 9:14 AM
Yes Eclipse wording ...
@frankfrank956 If works for you please tag such topic as Answered will help community
2020-07-29 9:23 AM
I don’t think I can do that as it isn’t my topic, I believe only frankfrank956 can do it.