cancel
Showing results for 
Search instead for 
Did you mean: 

How to fix this error will not fit in region `RAM_D1'

Kai_Satone
Senior

17:13:32 **** Incremental Build of configuration Debug for project LVGE_ex_code_H7 ****

make -j4 all

arm-none-eabi-gcc -o "LVGE_ex_code_H7.elf" @"objects.list" -mcpu=cortex-m7 -T"D:\stm32H7\LVGE_ex_code_H7\STM32H750VBTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="LVGE_ex_code_H7.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group

C:/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: LVGE_ex_code_H7.elf section `.bss' will not fit in region `RAM_D1'

C:/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: region `RAM_D1' overflowed by 488072 bytes

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:125: LVGE_ex_code_H7.elf] Error 1

"make -j4 all" terminated with exit code 2. Build might be incomplete.

 

17:13:35 Build Failed. 3 errors, 0 warnings. (took 3s.49ms)

 

 

 

/*
******************************************************************************
**
**  File        : LinkerScript.ld (debug in RAM dedicated)
**
**  Author      : STM32CubeIDE
**
**  Abstract    : Linker script for STM32H7 series
**                1024Kbytes RAM_EXEC and 544Kbytes RAM
**
**                Set heap size, stack size and stack location according
**                to application requirements.
**
**                Set memory bank area and size if external memory is used.
**
**  Target      : STMicroelectronics STM32
**
**  Distribution: The file is distributed as is, without any warranty
**                of any kind.
**
*****************************************************************************
** @attention
**
** Copyright (c) 2024 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
****************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(DTCMRAM) + LENGTH(DTCMRAM);    /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200;      /* required amount of heap  */
_Min_Stack_Size = 0x400; /* required amount of stack */

/* Specify the memory areas */
MEMORY
{
  RAM_EXEC (xrw)  : ORIGIN = 0x24000000, LENGTH = 1024K
  DTCMRAM (xrw)   : ORIGIN = 0x20000000, LENGTH = 128K
  RAM_D2 (xrw)    : ORIGIN = 0x30000000, LENGTH = 288K
  RAM_D3 (xrw)    : ORIGIN = 0x38000000, LENGTH = 64K
  ITCMRAM (xrw)   : ORIGIN = 0x00000000, LENGTH = 64K
}

/* Define output sections */
SECTIONS
{
  /* The startup code goes first into RAM_EXEC */
  .isr_vector :
  {
    . = ALIGN(4);
    KEEP(*(.isr_vector)) /* Startup code */
    . = ALIGN(4);
  } >RAM_EXEC

  /* The program code and other data goes into RAM_EXEC */
  .text :
  {
    . = ALIGN(4);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)
    *(.RamFunc)        /* .RamFunc sections */
    *(.RamFunc*)       /* .RamFunc* sections */

    KEEP (*(.init))
    KEEP (*(.fini))

    . = ALIGN(4);
    _etext = .;        /* define a global symbols at end of code */
  } >RAM_EXEC

  /* Constant data goes into RAM_EXEC */
  .rodata :
  {
    . = ALIGN(4);
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    . = ALIGN(4);
  } >RAM_EXEC

  .ARM.extab (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    *(.ARM.extab* .gnu.linkonce.armextab.*)
  } >RAM_EXEC
  .ARM (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
  } >RAM_EXEC

  .preinit_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array*))
    PROVIDE_HIDDEN (__preinit_array_end = .);
  } >RAM_EXEC

  .init_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array*))
    PROVIDE_HIDDEN (__init_array_end = .);
  } >RAM_EXEC

  .fini_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array*))
    PROVIDE_HIDDEN (__fini_array_end = .);
  } >RAM_EXEC

  /* used by the startup to initialize data */
  _sidata = LOADADDR(.data);

  /* Initialized data sections goes into RAM, load LMA copy after code */
  .data :
  {
    . = ALIGN(4);
    _sdata = .;        /* create a global symbol at data start */
    *(.data)           /* .data sections */
    *(.data*)          /* .data* sections */

    . = ALIGN(4);
    _edata = .;        /* define a global symbol at data end */
  } >DTCMRAM AT> RAM_EXEC

  /* Uninitialized data section */
  . = ALIGN(4);
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section */
    _sbss = .;         /* define a global symbol at bss start */
    __bss_start__ = _sbss;
    *(.bss)
    *(.bss*)
    *(COMMON)

    . = ALIGN(4);
    _ebss = .;         /* define a global symbol at bss end */
    __bss_end__ = _ebss;
  } >DTCMRAM

  /* User_heap_stack section, used to check that there is enough RAM left */
  ._user_heap_stack :
  {
    . = ALIGN(8);
    PROVIDE ( end = . );
    PROVIDE ( _end = . );
    . = . + _Min_Heap_Size;
    . = . + _Min_Stack_Size;
    . = ALIGN(8);
  } >DTCMRAM

  /* Remove information from the standard libraries */
  /DISCARD/ :
  {
    libc.a ( * )
    libm.a ( * )
    libgcc.a ( * )
  }

  .ARM.attributes 0 : { *(.ARM.attributes) }
}

 

 

10 REPLIES 10

Hello @Kai_Satone ,

Glad to hear you've solved the issue. Thank you for the feedback.

You need now to accept as solution the comment that answered or at least guided you to the solution.

Thanks

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.