2022-01-05 04:12 PM
Hello 🙂
I was trying to send some data to the console using USART1 (STM32F7508-DK).
With the following simple data there was no problem:
uint8_t data[] = "HELLO! \r\n";
HAL_UART_Transmit(&huart1, data, sizeof(data), 1000);
But when I try to display values using that code:
uint8_t pData = 0x80;
uint16_t tempData[64];
uint8_t convtempData[128];
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_StatusTypeDef ret = HAL_ERROR;
uint8_t ACCEL_ADDR;
ACCEL_ADDR = 0xD0;
ret = HAL_I2C_IsDeviceReady(&hi2c1, ACCEL_ADDR, 1, 100);
ret = HAL_I2C_Master_Transmit(&hi2c1, ACCEL_ADDR, &pData, 2, 50);
ret = HAL_I2C_Master_Receive(&hi2c1, ACCEL_ADDR | 0x01, convtempData, 128, 150);
print_to_console(convtempData);
}
And print _to_console() function look in that way:
void print_to_console(uint8_t* convtempData)
{
uint8_t space[] = " ";
for(int i = 0; i < sizeof(convtempData); i++)
{
HAL_UART_Transmit(&huart1, convtempData[i], sizeof(convtempData[i]), 1000);
HAL_UART_Transmit(&huart1, space, sizeof(space), 1000);
}
}
From console:
Also, it looks like program exits print _to_console() after 4th iteration (i=3) and goes to the int main () to while(1).
Does anyone knows how to solve it?
USART1 configuration (same configuration in the console):
2022-01-05 05:07 PM
Data Representation 101
The data in the array is in binary form used by the computer, if you want human readable ASCII decimal characters use sprintf(str,"%d". ..) or itoa()
2022-01-05 05:15 PM
In addition, use strlen instead of sizeof to avoid sending a null character (or more), at the end of each transmission.
2022-01-06 01:38 AM
@Community member @TDK Thank you for your answers 🙂 Indeed, I want to have human readable elements in the console.
Could you tell me how the correct syntax looks like?
I tried those 2 options:
void print_to_console(uint8_t* convtempData)
{
uint8_t space[] = " ";
for(int i = 0; i < 128; i++)
{
HAL_UART_Transmit(&huart1, itoa(convtempData[i]), strlen(convtempData[i]), 1000);
HAL_UART_Transmit(&huart1, space, sizeof(space), 1000);
}
}
And:
void print_to_console(uint8_t* convtempData)
{
char buffer[3] ;
for(int i = 0; i < 128; i++)
{
sprintf(buffer , "%u ",convtempData[i]);
printf("%s", buffer);
}
}
And unfortunately it didn't work :(
2022-01-06 03:14 AM
It looks like you need to spend some time studying the standard C string handling functions - this is standard C stuff, nothing specifically to do with STM32.
It is far easier to learn basic C skills on a PC or similar "conventional" computer - away from all the added complexities of embedded microcontrollers.
Here are some C learning & reference materials - including a free online textbook:
https://blog.antronics.co.uk/2011/08/08/so-youre-thinking-of-starting-with-c/
HAL_UART_Transmit( &huart1, itoa(convtempData[i]), strlen(convtempData[i]), 1000 );
Check the definition of itoa: eg, https://www.cplusplus.com/reference/cstdlib/itoa/ - you have to tell it where to store the string.
It's the length of that string that you need to tell HAL_UART_Transmit
strlen(convtempData[i]) won't work because convtempData[i] is not a string.
2022-01-06 06:05 AM
void print_to_console(uint8_t* convtempData)
{
char buffer[16] ;
for(int i = 0; i < 128; i++)
{
HAL_UART_Transmit(&huart1, buffer, sprintf(buffer, "%u ",convtempData[i]), 1000);
}
}