cancel
Showing results for 
Search instead for 
Did you mean: 

How to change the compiler version on CubeIde

DMukh.1
Associate
  1. If I want CubeIde to use a specific gnu arm version which is on my local system, should I just setup the build variable "gnu_arm_embedded_compiler_path" ? Is that enough?
  2. If I wish to check the current version that cube ide is using, how do I do that?

Sorry, maybe basic questions but would be of help. Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Evangelist III

Just use the toolchain manager. No need to tweak PATH; CubeIDE will ensure that the chosen toolchain is called.

0693W00000AM8YUQA1.png

View solution in original post

2 REPLIES 2
Pavel A.
Evangelist III

Just use the toolchain manager. No need to tweak PATH; CubeIDE will ensure that the chosen toolchain is called.

0693W00000AM8YUQA1.png

Cartu38 OpenDev
Lead II

@Pavel A.​  contribution is right one.

Please tag such post to answered as will help community to dig into valuable material more quickly. Thanks.