2019-11-04 2:12 AM
I was trying to flash my code into the STM32L0xx series controller, not a Evaluation board. When I did, it said the code has flashed that it was successfully done but when I disconnected the debugger ST-Link(GDB) and re-plug it to power the code did not run it needed a hardware reset to run this code. How can I control this reset to reset when hot plugged and should be done without any button or hardware reset. Only software reset must be done because of our application. The log from the console is below
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_FOH6Us.log
ST-LINK SN : 56FF6E067878545229500667
ST-LINK FW : V2J34S7
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x425
Device name : STM32L03x/L04x/L010
Flash size : 32 KBytes
Device type : MCU
Device CPU : Cortex-M0+
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_MkLRzZ.srec
File : ST-LINK_GDB_server_MkLRzZ.srec
Size : 6504 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 50]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.789
Verifying ...
Download verified successfully