cancel
Showing results for 
Search instead for 
Did you mean: 

How can I get a firmware for STEVAL-DPSLLCK1?

Sbaek.1
Associate

Hi, I am seung-woo.

I bought two STEVAL-DPSLLCK1. How can I get a firmware for STEVAL-DPSLLCK1?

In, STSW-DPSLLCK1 - STM32F334 full bridge LLC firmware package for STEVAL-DPSLLCK1 - STMicroelectronics

I was download "en.stsw-dpsllck1.zip". However, in the file, only one 55kb binary file.

How can I get a full project file?

Regards.

8 REPLIES 8
AShei.1
Associate

I'm looking for the same files.

I'd appreciate any help from ST side.

Thank you!

AMao.1
Associate

So u get the IAR/EWARM project file?

AVilk.1
Associate

Same problem. Couldnt find the files... Any help is very appreciated.

victagayun
Senior III

Hello ST,

Maybe you have forgotten to upload the files.

We are looking for the source code. It says in the manual like this:

0693W00000SvY5uQAF.png 

There seem to be no restrictions stated in the brief.

AB V.1
Associate II

I am also looking for the same. Appreciate any help from STM.

@AShei.1​ @AMao.1​  @[AVilk.1] Any of you got access to source code?

victagayun
Senior III

You can download the firmware at https://eds.st.com/llc/

0693W00000WKHLJQA5.png

AB V.1
Associate II

Thanks for pointing to the resource. Attaching the file here.

Archive has check sum errors and cannot be extracted. Same for archive from eds.st.com/llc

Do you have a working on?