2021-01-23 12:51 AM
2021-01-27 06:21 AM
Hello Markus,
I've already solved this problem. I missed a right manual, I could not find it at the STM site, but I found it anywhere in the internet few days ago: I have to connect the board via "User USB" to program access/program the flash! Now it works.
Sometimes it is very useful to have access to and to read the manuals.
Kind Regards,
Michael
2021-01-27 02:56 AM
Is this for any project you create or for this specific one?
Can you connect to the board if you're using the stand-alone CubeProgrammer? Available here.
2021-01-27 06:21 AM
Hello Markus,
I've already solved this problem. I missed a right manual, I could not find it at the STM site, but I found it anywhere in the internet few days ago: I have to connect the board via "User USB" to program access/program the flash! Now it works.
Sometimes it is very useful to have access to and to read the manuals.
Kind Regards,
Michael