2020-02-20 06:59 AM
2020-02-20 10:36 AM
2020-02-20 07:08 AM
It does "_64", doesn't it ?
And there are other architectures around, not only x86. Which can be 32 bit or 64 bit.
Usually, 64 bit systems/OSes support 32 bit application versions as well.
2020-02-20 08:05 AM
If it said i386 then you could expect the 32 bit version. Otherwise what @Ozone said.
2020-02-20 10:36 AM
2020-02-20 10:59 AM
Well, I would agree with that except I selected the Windows architechture version, so other architectures don't apply. Within windows, if you have a 64-bit system then the x86 folder is where the 32-bit applications go. So an application quoting both is (according to many other developers) compatible with both 32-bit and 64-bit Windows. There are many software programs where you select 64 or x86 versions. It does "x86" doesn't it ? No, it doesn't.
2020-02-20 11:27 AM
Thanks Piranha, a helpful response.
2020-02-20 01:31 PM
Buy a new system. There you go.
2020-02-21 01:04 AM
I did, and it worked! I bought a PicKit: v.much cheaper than a new laptop. Thanks, great suggestion :)
2020-02-21 07:16 AM
A new system *was* the recommendation you thanked Piranha for, but you went and got a PicKit? At least you didn't get an ICD-3
2020-02-29 06:57 AM
There is another better option - to choose some usable IDE instead of Eclipsoid. :)