cancel
Showing results for 
Search instead for 
Did you mean: 

Hello everyone, I am using STM32f105RC for my project in which I have to interface SD Card. But since in datasheet it says can be used. But do I have to use level conversion circuit also? Thanks in advance

KSing
Associate II

And also code it accordingly using stm32CubeIDE.

2 REPLIES 2

The SDIO interface and cards should be fine at 3.0 or 3.3V

For example circuits see EVAL series board schematics.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Okay, Thanx a lot.