2024-03-06 02:29 PM
Hi, I am trying to set up magnetic encoder from RLS. It is communicating over SPI, but I am having hard time setting it up. I am not sure if I am not using SPI correctly or setting the settings specificated for encoder. Encoders LED light keeps blinking, which means it is communicating correctly. Here is my code and settings:
Here is also screenshot of most of settings from datasheet (but here is the link to whole document
I am complitely beginer, so I apologize if I did simple mistakes. Thank you for help.
2024-03-12 01:23 PM
Got it working, all good