Skip to main content
Associate III
March 12, 2024
Solved

STM32CubeIDE placing variable on specific addres in external SDRAM

  • March 12, 2024
  • 3 replies
  • 2045 views

Hello,

i need help how to edit linker file for placing array on specific address in external SDRAM connected via FMC.

I'm working with 7" TFT 800x480 @ 24bpp via LTDC controller and i have configuration 2 layers and both double buffered. So in HW is connected external SDRAM 8MB four banks (2MBx4). I would like to use each bank for one buffer as recommended in AN4861 https://www.st.com/resource/en/application_note/an4861-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf.

I added SDRAM and SDRAM section into linker script as follows:

SDRAM (rwx) : ORIGIN = 0xC0000000, LENGTH = 8192K

...

...

.sdram (NOLOAD) :
{
. = ALIGN(4);
*(.sdram .sdram.*)
} > SDRAM

 

But i don't know how to place four buffers into start address of each SDRAM bank.

I tried to create 4 SDRAM sections instead of one:

SDRAM0 (rwx) : ORIGIN = 0xC0000000, LENGTH = 2048K
SDRAM1 (rwx) : ORIGIN = 0xC0200000, LENGTH = 2048K
SDRAM2 (rwx) : ORIGIN = 0xC0400000, LENGTH = 2048K
SDRAM3 (rwx) : ORIGIN = 0xC0600000, LENGTH = 2048K

...

...

/* external SDRAM0 */
.sdram0 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram0 .sdram0.*)
} > SDRAM0

/* external SDRAM1 */
.sdram1 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram1 .sdram1.*)
} > SDRAM1

/* external SDRAM2 */
.sdram2 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram2 .sdram2.*)
} > SDRAM2

/* external SDRAM3 */
.sdram3 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram3 .sdram3.*)
} > SDRAM3

 

and declare variables as:

uint32_t lcd_buffer0[288000] __attribute__((section(".sdram0")));
uint32_t lcd_buffer1[288000] __attribute__((section(".sdram1")));
uint32_t lcd_buffer2[288000] __attribute__((section(".sdram2")));
uint32_t lcd_buffer3[288000] __attribute__((section(".sdram3")));

 

But i don't know if it's correct approach.

 

Can you help me how to do it?

This topic has been closed for replies.
Best answer by TDK

That is the correct approach. Does it compile and work? Might be missing some subtle syntax but the idea is correct.

3 replies

TDK
TDKBest answer
March 12, 2024

That is the correct approach. Does it compile and work? Might be missing some subtle syntax but the idea is correct.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Petr3Author
Associate III
March 12, 2024

Yes, it seems to work fine. List file shows, that buffers are placed on correct adddres in external SDRAM.

Pavel A.
March 12, 2024

@Petr3 You don't even need to touch the link script. Just define the addresses as standard C pointers with absolute values. For example 

#define lcd_buffer0 ((uint8_t*)0xC0000000)
....
#define lcd_buffer3 ((uint8_t*)0xC0600000)