2024-08-07 06:09 PM
Hi,
I installed GitHub Desktop and created a local repository which resides inside a an STM32 CubeIDE project.
I can modify any of the .c or .h files with any editor (notepad, notepad++, wordpad, etc) and the changes appear immediately in GitHub Desktop. But if I edit the same file/s with CubeIDE editor the changes do not appear at all on GitHub Desktop. i.e. GitHub Desktop does not show that the file (or any file) has been changed.
Does anybody have any idea why?
2024-08-07 07:47 PM
Duplicate:
Github Desktop not showing any file changes ONLY w... - STMicroelectronics Community