2024-02-26
07:21 AM
- last edited on
2024-07-04
06:02 AM
by
Lina DABASINSKAITE
Dear Sirs
I am having a problem using FreeRTOS and USB on H7 series MCU. The IDE gives “Hard Fault” when I debug the project. See image below.
The environments are :
STM32CubeIDE: Version: 1.14.0, Build: 19471_20231121_1200 (UTC)
Target: NUCLEO-H743ZI2
Enclosed herewith are the two “ioc” files.
FreeRTOS_USB1.ioc is for the project without initialization to the USB and it is working fine.
FreeRTOS_USB.ioc is for the project with the initialization to the USB and it is giving my Hard Fault.
Your help and assistance are highly appreciated.
Best Regards
Dr Reyah Abdula
2024-07-19 03:52 AM
Hi @RAbdu.1542
Do you still have the same issue if yes, please consider attaching your IOC file.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-27 02:13 AM
Hi FBL
Thank you for the reply. Yes, I am still having the problem. I already attached the IOC files above.
Regards