cancel
Showing results for 
Search instead for 
Did you mean: 

Folders missing

Ak1893
Associate

Hello everyone,
I have the problem that only these 2 files are displayed on my Project Explorer. Once testpro and testpro.ioc all other files are missing, for example the C program main.c. My question is can someone help me to fix this problem?

1 ACCEPTED SOLUTION

Accepted Solutions

Okay so MacOS.

Not sure how the screenshot helps here. Did you try the project menu? Show it

> it says that the code is being generated

Perhaps you need to log in or download the relevant software packages in Help -> Manage Embedded...

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

5 REPLIES 5
TDK
Guru

Code must be generated after you configure the IOC file. To generate code, go to Project -> Generate Code

TDK_0-1740336628691.png

 

If you feel a post has answered your question, please click "Accept as Solution".

If i go to project, there is no generate code. And if i go to the bar at the top, it says that the code is being generated, but then nothing comes up.

welcome to the forum.

Please see: How to write your question to maximize your chances to find a solution.

 

You haven't given what CubeIDE version you're using, or details of your development Host system.

Okay so MacOS.

Not sure how the screenshot helps here. Did you try the project menu? Show it

> it says that the code is being generated

Perhaps you need to log in or download the relevant software packages in Help -> Manage Embedded...

If you feel a post has answered your question, please click "Accept as Solution".

Ok, I downloaded the software packages. Now it works. Thank you for your help