2021-09-08 12:36 AM
Hi ,
i am new to some of the peripherals of STM32 controllers...
I am using STM32L151RCT6 MCU in STMCube IDE for my application..
My requirement is like i need to receive the new firmware binary file via Y modem and need to write into the flash and need to run that application by sending one of the CLI from the UART..
I tried with some examples but not getting proper working of Y modem for receiving the binary file..
Please suggest me if any example codes along with reference document, it will be helpful for me..
it is very much necessary for me....
2021-09-08 1:49 AM
Hello,
you have some ymodem implementations in the firmware packages:
STM32Cube_FW_F1_V1.8.4\Projects\STM3210E_EVAL\Applications\IAP\IAP_Main
STM32Cube_FW_F0_V1.11.3\Projects\STM32091C_EVAL\Applications\IAP\IAP_Main
STM32Cube_FW_F4_V1.26.2\Projects\STM324x9I_EVAL\Applications\IAP\IAP_Main
There is a readme.txt file in those examples.
2021-09-09 12:20 AM
Hi Mike,
Thanks for your reply , based on the above examples i prepared one project for STM32L151RCT6 MCU and i loaded it.
passing the binary file from the Y modem Tera term , it is receiving half of the file and stopped shown bellow.
i tried the uart baud rate for both 9600 and 115200 both are showing same behaviour , i am not getting what is problem..
please help me for this .. it is needed for me.
consider the attached y modem function.
2021-09-09 12:22 AM
2021-09-09 12:24 AM
It is stopping as shown above
2021-09-09 12:27 AM
/**
******************************************************************************
* @file IAP_Main/Inc/flash_if.h
* @author MCD Application Team
* @version 1.0.0
* @date 8-April-2015
* @brief This file provides all the headers of the flash_if functions.
******************************************************************************
* @attention
*
* <h2><center>© COPYRIGHT(c) 2015 STMicroelectronics</center></h2>
*
* Redistribution and use in source and binary forms, with or without modification,
* are permitted provided that the following conditions are met:
* 1. Redistributions of source code must retain the above copyright notice,
* this list of conditions and the following disclaimer.
* 2. Redistributions in binary form must reproduce the above copyright notice,
* this list of conditions and the following disclaimer in the documentation
* and/or other materials provided with the distribution.
* 3. Neither the name of STMicroelectronics nor the names of its contributors
* may be used to endorse or promote products derived from this software
* without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
* IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
* DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
* FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
* DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
* CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
* OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
******************************************************************************
*/
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __FLASH_IF_H
#define __FLASH_IF_H
/* Includes ------------------------------------------------------------------*/
#include "stm32l1xx_hal.h"
#include "stm32l1xx_hal_conf.h"
/* Exported types ------------------------------------------------------------*/
/* Exported constants --------------------------------------------------------*/
/* Error code */
enum
{
FLASHIF_OK = 0,
FLASHIF_ERASEKO,
FLASHIF_WRITINGCTRL_ERROR,
FLASHIF_WRITING_ERROR,
FLASHIF_PROTECTION_ERRROR
};
/* protection type */
enum{
FLASHIF_PROTECTION_NONE = 0,
FLASHIF_PROTECTION_PCROPENABLED = 0x1,
FLASHIF_PROTECTION_WRPENABLED = 0x2,
FLASHIF_PROTECTION_RDPENABLED = 0x4,
};
/* protection update */
enum {
FLASHIF_WRP_ENABLE,
FLASHIF_WRP_DISABLE
};
/* Define the address from where user application will be loaded.
Note: this area is reserved for the IAP code */
#define FLASH_PAGE_STEP FLASH_PAGE_SIZE /* Size of page : 2 Kbytes */
#define APPLICATION_ADDRESS (uint32_t)0x08004000 /* Start user code address: ADDR_FLASH_PAGE_8 */
/* Notable Flash addresses */
#define FLASH_START_BANK1 ((uint32_t)0x08000000)
#define WORDS_IN_HALF_PAGE ((uint32_t)16)
#define FLASH_HALF_PAGE_SIZE ((uint32_t)WORDS_IN_HALF_PAGE*4)
#define FLASH_LAST_SECTOR_BANK1 ((uint32_t)0x08017000)
#define FLASH_LAST_PAGE_BANK1 ((uint32_t)0x08017F00)
#define FLASH_END_BANK1 ((uint32_t)0x08017FFF)
#define FLASH_START_BANK2 ((uint32_t)0x08018000)
#define USER_FLASH_END_ADDRESS ((uint32_t)0x08030000)
#define FLASH_BANK1_MASK ((uint32_t)0xF0FFFFFF)
/* Define the user application size */
#define USER_FLASH_SIZE ((uint32_t)0x00003000) /* Small default template application */
/* Exported macro ------------------------------------------------------------*/
/* ABSoulute value */
#define ABS_RETURN(x,y) (((x) < (y)) ? (y) : (x))
/* Get the number of sectors from where the user program will be loaded */
#define FLASH_SECTOR_NUMBER ((uint32_t)(ABS_RETURN(APPLICATION_ADDRESS,FLASH_START_BANK1))>>12)
/* Compute the mask to test if the Flash memory, where the user program will be
loaded, is write protected */
#define FLASH_PROTECTED_SECTORS (~(uint32_t)((1 << FLASH_SECTOR_NUMBER) - 1))
/* Exported functions ------------------------------------------------------- */
void FLASH_If_Init(void);
uint32_t FLASH_If_Erase(uint32_t StartSector);
uint32_t FLASH_If_GetWriteProtectionStatus(void);
uint32_t FLASH_If_Write(uint32_t destination, uint32_t *p_source, uint32_t length);
uint32_t FLASH_If_WriteProtectionConfig(uint32_t protectionstate);
void FLASH_ClearFlag(uint32_t FLASH_FLAG);
#endif /* __FLASH_IF_H */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
These are flash memory definitions
2021-09-09 1:13 AM
Hello,
Please, try with Teraterm version 4.85, just to check whether it works. I know that later Teraterm ymodem implementation has changed a bit.
You'll probably have to learn a bit about ymodem protocol too to see why it is stalling.
2021-09-09 6:01 AM
Hi,
Thanks for reply , i tried with same version of Tera term what you suggested but not solved the issue..
is it related to flash programming ? or any address assigning?