File tabs in STM32CubeIDE broken
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-06-22 11:29 AM
I am using 2 separate workspaces, one which I created some years ago with an older version (workspace #1), and a newer one (workspace #2). Recently I imported an older project into workspace #1, and I am encountering the issue that the file tabs are broken when I open several files. When I hover the cursor over the tabs, then the tabs become blank, see attached screen shot. The issue does not occur when switching to workspace #2. I tried to re-initialize the workspace #1 by deleting the metadata and re-importing the project, but it did not help. I did not try to re-create the project from scratch, because that is a lot of work. Is there anything in the workspace or the project which can cause this erratic behavior of the IDE?
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-06-22 11:27 PM
Hello there,
Just so I get a clear understanding, you imported an older project into the old workspace (workspace #1) and that old project was never used with the old workspace previously?
Are there different versions of STM32CubeIDE using these two different workspaces?
In the workspace you have a .metadata map which contains a .log file which I could take a look at, perhaps it will show me something.
You could also try to create a new workspace and import the project there, it's a more thorough way of "deleting metadata and re-importing" in a way, could be useful to know if it helps the issue or not.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-06-23 12:09 PM
Hello Markus,
I actually started with adding the workspace created with an older version of the IDE to the new version. That's when I started to encounter the issue.
I now deleted the entire workspace, let the IDE re-create it from scratch, and then re-imported the project to the newly created workspace. Still the same issue. When hovering over the file tabs, the tab becomes blank. If you hover over the X next to the file name, usually the black X should be replaced by a red X. This does not happen, and I am getting a section of an icon representing the .c file icon, which is placed in front of the file name. Something seems to be broken with the icons.
I also tried to create a new project from an example project in this workspace, and I am getting the same issue. Also a newly created blank project has the issue.
Something is broken with the handling of the tabs, and it depends on the workspace if the issue occurs or not. Any ideas?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-27 9:49 AM
AWies, I don't know if you solved this? I had the same issue and had trouble finding a solution. I didn't find any actually. Finally, playing randomly around with the Compability settings I got the problem to stop. I ticked "on" these two settings in DPI settings. No idea what it does or means, but it worked.