cancel
Showing results for 
Search instead for 
Did you mean: 

Fault Analyzer - No Hard Fault info; No Toolbar (IDE v1.13.0)

Andrew Neil
Evangelist III

STM32F030.

STM32CubeIDE v1.13.0.

I've hit a Hard Fault:

AndrewNeil_3-1721139450921.png

But the Fault Analyzer tells me nothing:

AndrewNeil_0-1721139114360.png

Where's all the other info?

AndrewNeil_1-1721139225361.png

Also, I don't see the promised toolbar buttons anywhere:

AndrewNeil_2-1721139270325.png

 

See also: https://community.st.com/t5/stm32cubeide-mcus/fault-analyzer-toolbar-missing/m-p/677402/highlight/true#M27539

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Andrew Neil ,

Fault analyzer toolbar is no more available but not the fault analyzer feature, which is still available but, in your case, you are working on a cortex M0 based microcontroller (STM32F0) so no fault related registers are available and no fault analyzer view subsequently for other cortex M4 -M33 -M7 you can still have the full view of the fault-analyzer.
Regards 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
Mahmoud Ben Romdhane
ST Employee

Hello @Andrew Neil ,

First let me thank you for posting.

There was a consensus to remove this feature Fault Analyzer toolbar from STM32CubeIDE and a change request has been raised to update the Release Note and the User Manual under this Ticket: 174829.

Thanks.

Mahmoud

 


@Mahmoud Ben Romdhane wrote:

There was a consensus to remove this feature from STM32CubeIDE


Really - why?!

When was it removed?


@Andrew Neil wrote:

@Mahmoud Ben Romdhane wrote:

There was a consensus to remove this feature from STM32CubeIDE


Really - why?!

When was it removed?


@Mahmoud Ben Romdhane Any update on this?

If it is the case, then this knowledge base article needs to be updated:

https://community.st.com/t5/stm32-mcus/how-to-debug-a-hardfault-on-an-arm-cortex-m-stm32/ta-p/672235

@Lina_DABASINSKAITE 

 

Hi @Andrew Neil , thanks for brining this us. We will look into this with the author of this article. Greetings!


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks.

So are you confirming that the Fault Analyser has, in fact, been deliberately removed from CubeIDE?

If so, why?

Me too. I'd like to know what the rationale is for removing a useful tool from the IDE.

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.

Hello @Andrew Neil ,

Fault analyzer toolbar is no more available but not the fault analyzer feature, which is still available but, in your case, you are working on a cortex M0 based microcontroller (STM32F0) so no fault related registers are available and no fault analyzer view subsequently for other cortex M4 -M33 -M7 you can still have the full view of the fault-analyzer.
Regards 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.