2019-05-29 1:24 PM
The STM32CubeIDE version 1.0.0 is installed in my computer. When creating a new STM32 project with STM32F103ZE, IDE pops "Open Associated Perspective?" window. After clicking Yes, Downloading selected software pack.. window will show "Problem during Download and/or ...". Error message is "Error downloading the following files: stm32cube_fw_f1_v170.zip(Target directory already exists)". Is it a real problem, or just a confusing message?
2019-06-03 2:29 AM
Does the project get generated after you receive the "Problem during Download" error message or not? Does the firmware pack get installed or do you already have it installed?
2019-06-04 6:03 AM
Yes, the project is generated indeed, and the firmware pack get installed also.
The question is this problem always happens when I create a new project with the same MCU. I understand it when creating a new project with a new MCU first time, because the firmware pack might not be there. However, I am confused by this error when creating another project with the same MCU, because the firmware pack has been installed successfully with the previous project. So, I doubt whether the project is generated correctly.
I attach the procedure I take for your reference.
Thanks