STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1087 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 471 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

how to use st link and connect GDB server in cube Ide

 hi, I'm using STM32CubeIDE 1.3.1 and trying to execute some programs. but there's a this message. it seems the problem relay upgrading st link and GDB server but I don't know how to solve this. do anyone have the same problem? I'm using STM32CubeID...

0693W000001shWbQAI.png
T22 by Associate II
  • 2351 Views
  • 4 replies
  • 0 kudos

Resolved! STM32cubeide how to display variables in hex format?

When debugging using SWD if I stop at a breakpoint to check the value of a variable, the variable value is displayed in decimal. This is really annoying.How do I change the environment to permanently display variable values in hex when I hover over t...

Support from ST is dead?

I first reported bugs related to the STM32CubeIDE SWV viewer on February 25th. No ST employees responded to it or were considered.I also opened a topic for almost three weeks, but the result is the same: they don't even try to deal with the topic.The...

PTiha by Senior
  • 4555 Views
  • 13 replies
  • 0 kudos

How do I configure STM32CubeIDE to upload optimized code

A section of my code is CPU intensive and is starting to affect user interaction. I need to optimize this part, or build it optimized and upload it into the device from the IDE.I know how to upload code using the STM32CubeProgrammer, but using 2 UIs ...

Radiofan by Associate II
  • 3006 Views
  • 6 replies
  • 0 kudos