cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to list external Loader

ALomb.1
Associate III

I try to add external loader to C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin\ExternalLoader

In debug configuration, check ExternalLodaer and than press Scan.

The scan fail with message "Failed to list external Loader"

If I remove the external loader that I added the scan work fine.

The exetrnal loader that I try to add is MX25L6433F_GFX01M2_STM32G0.stldr from X-CUBE-DISPLAY pack.

STM32CubeIDE Version: 1.8.0

20 REPLIES 20
Karim BEN BELGACEM
ST Employee

This has been fixed with the new X-CUBE-DISPLAY 2.1.0 release available from here : X-CUBE-DISPLAY - Display module software expansion for STM32Cube - STMicroelectronics