ethernet communication between stm32h745 nucleo boards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-06-18 12:39 AM
Hello everyone, i want to send ethernet packet from one stm32h745 nucleo board to another board. i connect the boards with rj45 biderictional cable, and i use the eth in both boards(one to transmit and one to transmit). i try to debug the program of the transmitter board and i see that after one transmitted packet(which i know that transmitted because status_ok returned from func) i get status_error on transmit, and i do not know why. i am begginer so i do not know how to approch this problem, maybe i misunderstand some basic concept about ethernet communication or something else. i attach my main loop for help. thanks!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-06-18 1:02 AM
Hi, I did tests with the F407 and the LAN8720, but I used the computer to monitor the sending and receiving, I used this tool to test: Hercules SETUP utility.
- Complete support for Windows 7, 8, 8.1 and 10
- All basic TCP and UDP utilities in one file, no installation required (just one .EXE file)
- Implemented Serial Port Terminal is working with the Virtual Serial Ports (COM12 for example). You can check and control all serial port lines (CTS, RTS, DTR, DSR, RI, CD)
- Simple TCP client (like the Hyperterminal) with the TEA support, view format, file transfers, macros..
- Easy to use TCP Server with the TEA support, view format, file transfers, macros..
- Hercules contains simple UDP/IP "Terminal" with view formats, echo, file transfers, macros..
- Support the NVT (Network Virtual Terminal) in the Test mode tab, as like as NVT debuging features..
- Using Telnet extended with NVT allows serial port configuration (RFC2217), device identification, confirmation of data sequence, etc.
- It's FREEWARE you can use and share this software free
See too: [This page will explain points to think about when capturing packets from Ethernet networks]